Hi!
I'm in the beginning of a project at Lund University where we will use a BLDC motor to drive a gearbox. We want to drive it the motor on a low rpm, around 200 rpm. I would like to be able to use a MCU to control the motor (via the driver). A magnetic encoder (as5048) will be used for feedback. The motor that will be used is the following:
I have seen several projects online where the DRV8305 is used for similar applications.
My question is if there are any of TI's drivers that are better suited for the application?
Best regards / Christoffer