Other Parts Discussed in Thread: DRV8711
Hello,
I have few questions and i appreciate any help you can offer.
Timing:
I am thinking to use your DRV8873-Q1 to drive an inductive load where the inductor current will go between positive current to negative current. I am interested to know how fast can the H-bridge switched once it received a signal to change direction? For my project the maximum allowed time to switch from off to completely on between the bridges is 5us. I saw on the datasheet, it has a deadtime of only 500ns, min 1.2u propagation delay, and maximum slew rate of 53.2V/us. This puts the total dead time of at 500ns+1.2us+1us*2= 3.7us. Is the slew rate for rise and fall the same and is this the correct calculation for total switch time?
Max Current:
When does the CURRENT REGULATION Itrip play a role in the device. Will it prevent me operating the device over Itrip current but less than Iocp?
Alternative part:
Do you have parts you can recommend that will operate 15A and 50V?
Thanks,
JZ