Other Parts Discussed in Thread: EK-TM4C129EXL, , DRV8323
Good morning,
I'm using a DRV8323RS with 1xPWM mode and Hall Sensors feedbacks using a BOOSTXL-DRV8323RS board connected to a EK-TM4C129EXL connected via SPI and with the classical lines (nBrake, Dir, Cal, Enable, PWM and NFault).
Everything works fine apart in one situation: if I mechanically lock for a moment the motor sometime the drv8323 stops giving PWM output on the Gates. In this situation and I cannot restart the motor even driving low the NBrake line, or the enable line etc. The only possibility to restart the motor is to give a mechanical start spin to the rotor manually. Moreover the Fault Status Register 1 remains at 0.
Given the fact that in our final application it could be possible that the motor will get locked in some situations, could you please let me know why this happened and what could be the solution?
Thank you very much in advance for your help.
Best Regards,
Carlo