Hi Engineering Friends,
I plan to purchase and use the following vibration motor. The spec sheet is linked below.
https://pmdri.zendesk.com/attachments/token/TJv5tm0hqPpizSZ1vRiIWhdGl/?name=307-103.005-datasheet.pdf
I need help identifying what I will need to activate the vibration motors. The following is what I have in mind.
1. I will need to drive the Model 307-103.005 through its full range of frequencies and amplitudes. For example, at 100Hz. I would like to be able to control the frequency and amplitude, and the duration of vibration.
2. I would like to start (and stop) the vibration using an analog TTL voltage input. For example, 0 volts = no vibration; 5 volts = vibration at specified setting.
3. I would like to be able to activate two or more of the Model 307-103.005 at the very same time.
4. I will need extension wires to connect to the Model 307-103.005.
Thank you for your guidance.
-Michael