The two boards are connected by row pins. The control board is on the upper layer and the power board is on the lower layer. The power supply voltage waveform before enabling drv8301 is as follows
The power supply voltage waveform after enabling drv8301 is as follows
The power supply we use for testing is the aircraft model battery.
Why is this kind of power supply voltage noise extremely serious?
Regards,
-Beyso