This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2510-Q1: Value of capacitance of supply

Part Number: DRV2510-Q1

Hi teams,

I have a question about the supply capacitor.

From the table8. in datasheet of DRV2510.

The typical value of supply capacitor compose of a 22uf, a 10uf and a 0.1uF capacitor.

However, 22uf and two ceramic capacitor of 220pF to 1uF and 100nF to 1uF are recommended as the bulk bypass capacitor in 8.2.1.2.2.

It seems the 10uF capacitor is not necessary for the VDD.

I don't understant why they are differenct.

Can I have more information about that.

Best Regards,

Yun Lin