This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8881PEVM: I can not properly install the slvc629\DRV8881PEVM Software Files\GUI\DRV8881PEVM_installer

Part Number: DRV8881PEVM


Dear Team members,

Thanks for any suggestions or discussion about my problem below.

I just received the motor driver board DRV8881PEVM. I download the software package 'slvc629'.

I tried to install the "GUIComposerApp-v1.0.setup-win_2.0.3" and find the following problem.  2 windows 10 computer are already tried but get the same problem.

My system information is as followed:

Windows 10 Pro: @2019 Microsoft Corporation.

Processor: Intel(R) Core(TM) i7-6700K CPU@ 4.00GHz 4.01 GHz

RAM: 64.0GB

System type: 64-bit Operating System, x64-based processor

Thanks a lot for all your help!

Best regards,

John Ding