Hi,
In page 41 of datasheet. Itrip is shown set as 6.5A and Iipropi is 1/1100 and max voltage can be 5V so Rsense should be 700R but it is shown as 1.5K. is my calculation correct or should i Use 1.5K only
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
In page 41 of datasheet. Itrip is shown set as 6.5A and Iipropi is 1/1100 and max voltage can be 5V so Rsense should be 700R but it is shown as 1.5K. is my calculation correct or should i Use 1.5K only