This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8881: how to calculate power consumption of step motor and driver IC?

Genius 3900 points
Part Number: DRV8881
Other Parts Discussed in Thread: OPA564, , DRV8889-Q1

Hi there,

we are designing a simple 2-phase step motor driver. Motor spec is below. 

We are considering design TWO demo boards using different Driving solution: PWM voltage drive(DRV8881) and linear current drive(howland current source with OPA564) , both open-loop control. 

the current freq. in motor coil would be f_max=500HZ sine wave, and current amplitude <500mA as required by motor coil spec. Power supply of driver will be +/-10V.

A simulation may help, but I hope to learn the math in this :

(1) How should we  calculate  the power consumption of step motor   

(2) How should we calculate  the power consumption of PWM driver IC DRV8881 and linear driver OPA564? Linear SCH is below for reference while PWM SCH is in develeping. 

Thanks very much.