Hello team,
I would like to confirm/have the question below. Could you please support those?
1: Using Aout/Bout independently, can we change the decay mode during controlling the motor?
For instance, while Aout is in operation, change the mode to fast, and while Bout is in operation, change the mode to slow.
2: Based on the datasheet, Mixed decay is open, Logic High is above 2.0V, and Logic Low is below 0.8V.
The customer is thinking if the logic voltage is between 0.8 and 2.0V, it should enter mixed decay. Is this correct?
Best Regards,
Kazuki Kitajima