Hi,
I see in DRV8308EVM's Clock PWM Mode, PWM clock frequency is around 24KHz and duty cycle is around 26.8%. I want to use Clock PWM Mode for Closed-Loop Speed Control.
It is observed that at higher motor torque need, motor speed is reduced from 1500rpm to 1400rpm as it is a open loop control system.
How to make Closed-Loop Speed Control in Clock PWM Mode? Is this can be achieved by varying duty cycle of 24KHz CLKIN?