This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If a BLDC application is using a single shunt, (a) what is the best procedure for connecting the unused current sense amplifiers? (b) If the customer wants to use one of the current sense amplifiers for a function other than motor current sensing, would that be okay?
Thank you!
Lenio,
For an unused CSA we recommend the following:
All CSA inputs (SPC/SNC) to GND
SOx - Output of CSA floating
The CSA should not be used for a different purpose because the SPx pin is also used for the source connection and discharge path for the Low Side FET gate. The unused CSA SPx and SNx should be connected to GND as well as the source pin of the low side FET.
Regards,
-Adam
I thought the sources of all three low side MOSFET's could be connected to the shunt and that connected to one of the CSA's. Based on what you are saying, the shunt is connected to only one of the bridges. Can you please confirm?
Lenio,
Assuming you are using the B channel CSA, I would connect SPA/SNA/SNB/SPC/SNC to the GND side of the sense resistor. Only SPB will be connected to the top side of the sense resistor.
The source connection of all three low side FETs will be common and connected to SPB and the top of the sense resistor.
Regards,
-Adam