This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8825: Holding Current

Part Number: DRV8825
Other Parts Discussed in Thread: DRV8424

Hi Sir 

I use GPIO to change xVref voltage and IFS current 

TB_HOLD=H current is 349.7mA

TB_HOLD=L current is 773.8mA 

When I change TB_HOLD from low to high ,but the current still keep 773.8mA 

Have anything need to take care ? 

PS. When I set xVref voltage up to 1V,the issue is still exist 

This issue only happen on mixed decay mode , fast decay mode is workable 

Yellow is TB_HOLD

Green is DIR

Red is output current 

below figure is abnormal ,should be 349.7mA (H) not 773.8mA 

  • Kaile,

    Would you help me check the following items:

    1. Would you check xVREF voltage to replace "DIR" in your scope picture?

    2. If you keep sending STEP signal, does the full scale current change?

    3. "This issue only happen on mixed decay mode , fast decay mode is workable". How about slow decay? If we wait for one minute, is the current still kept at 773.8mA?

  • Hi Wang 

    CH1 (Yellow): TB_HOLD

    CH2 (Green): xVREF

    CH3 (Blue): TB_STEP

    CH4 (Red): output current

    Fast decay : OK

    Slow decay : NG

    Mixed decay : NG

  • Kaile,

    Thank you for the detail waveform comparison.  For the test waveform, we can see slow decay and mixed decay can not bring the output current back to reference voltage setting.

    The slow decay just turns on both high side FETs or both low side FETs which gives a very low voltage across the motor winding. The output winding current may drop very slow with slow decay mode.

    In tblank time, DRV8825 doesn't do the current regulation. On the slow decay zoom in waveform, the output current is driven up too much during the blanking time, the slow decay can not bring the current down quickly enough. The next switching cycle's tblank time, the output current keeps being driven up.  That is why you see the peak current is higher than the regulation point.

    Mixed decay occurs only if the current through the winding is decreasing (per the indexer step table); if the current is increasing, then slow decay is used. So, if the current is stopped in the rising edge, the output current could also be higher than the regulation point.

  • Hi Wang 

    I know TI release many new motor driver solution 

    May I know the new one still have this kind of issue ?

    DRV8424? Smart tune ?

  • Kaile,

    The new motor driver has smart tune decay which can automatically adjust the fast decay and slow decay percentage to avoid this issue.