Hello,
Q1:
From "Tuning Gide(SLOU395D)",
"Theoretically, we should choose the threshold to be as small as possible, because we can resynchronize the motor with lower speed.".
What is "resynchronize"? Please let me know detail of "resynchronize".
Q2:
From "Tuning Gide(SLOU395D)",
"Unless the application requires two-direction spinning or it is possible for the motor to have reserve speed before startup, the Enable Reverse Drive function and Brake function should be disabled.".
If motor has rotation by inertia, I think that I can setting Reverce Drive. Is my idea correct?
Q3:
From display for number of rotations on GUI,
I am using a 12-pole motor and I have entered 12 in the Pole field, but the value deviates from the actual motor speed.
If TI has how to fix that please let me know it.
Best regards,
ACGUY