Other Parts Discussed in Thread: DRV8601, DRV2603
Hello Guys,
Good day.
Our customer is planning to use DRV2605 in their design. It says that the DRV2605 use i2c for the playback engine to store pre-loaded waveforms and play them. Is it required to use i2c and is it required to store pre-loaded waveforms? Or can the i2c aspect be completely disregarded for this device to operate?
Also, they want to run their LRA at 0.6Vrms, how do they configure DRV2605 (or DRV8601) to drive the LRA at 0.6V RMS?
Thanks in advance!
Art