Hi Team,
The customer is experiencing below issue and needs your help.
When one of the PWM waves is given and enabled by the MCU, all three items are output. Measured by an oscilloscope, the three-phase enable terminal has irregular high-level signals, and the PWM input terminal also has abnormal high-level PWM waveforms. There is no problem in separately testing the PWM wave and EN signal given by the MCU, but the above abnormality occurs when put together.
Before this phenomenon occurred, the drive had a normal output. But after the above-mentioned abnormality, there was no normal output.
Customer would like to know:
What is the main reason for the above phenomenon? MCU is powered by 3.3V, DRV8313 is powered by 25V, but there is no common ground between the two. Is it caused by this? Does the drive ground and MCU ground need to be connected together?
Thanks,
Annie