My question is related to the unused SNx pins when using only SNA and SPA and a single sense resistor on my three phase bridge. I left them disconnected in my prototype board then relaized that at least SPB and SPC should be tied to the commong source point on the bottom FETS (the top of the sense resistor node) if the VDS over current sense is enabled. My question is if VDS over current sense is disable (pulled to VDD on the 8353RH) do they still need to be connected? I had things working for a brief period then killed my chip with too much gate drive (I suspect). I am getting ready to bring the next board up but before I do I want to understand if I need the source sense SPB and SBC tied to the proper source point or if I can leave them as no connects (IF the VDS over current sense is disabled)? I can see that if the VDS overcurrent sense was enabled and those pins were left floating bad things would happen and a fault would be likely.
Also what about the actual amplifier outputs for the sense resistors, do they just pass on the amplified analog sensed voltage or is there any other internal fault detection that those outputs could trigger? . This goes to my quesiton above and is related to leaving the other side of the amp input left unconnected (SNB and SNC). Will that cause any issues? I can't see where it would but I want to make sure.
Thanks,
Ross