This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10983: I2C Mode Speed Control

Part Number: DRV10983


Hi team,

When SpdCtrl [8] is written to the SpeedCtrl2 register, the data is stored, but the output is not changed. Why there is a buffer of SpdCtrl [8]? When will the SpdCtrl [8] of speed command be updated?

  • Hi Naizeng,

    The reason why data written in SpeedCtrl2 register is stored and not changed is because bit 9 of SpdCtrl is the MSB and this MSB should be written first before writing the LSB. Only after writing LSB, device updates speed command.

    Regards,

    Vishnu.