This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8705-Q1: How can we control speed and direction of motor using in H- bridge for PWM mode

Part Number: DRV8705-Q1

How can we control speed and direction of motor using in  H- bridge for PWM mode as PH/En both pin takes input PWM 

which PWM  can control control speed EN or PH pin

  • Hi,

    If you are using PH/EN control mode, you can vary the duty cycle of the EN pin to control the speed. You can also control the direction by changing the PH pin value. I suggest looking at table 5 of the datasheet to look at the control truth table. 

    If you are using PWM control mode, you can vary the duty cycle of both IN1 and IN2 to control the speed and direction. I suggest looking at table 6 to look at the control truth table.