This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8323: Using the INLC input pin to brake a BLDC motor

Part Number: DRV8323


Hello,

I am currently using the INLC pin on the DRV8323 as a hardwired brake for our BLDC motor.

A question has come up as we look into functional safety on our machine if the INLC pin is braking the motor directly, or if the INLC pin goes through the DRV software to brake the motor. 

Can someone clarify how the INLC brake pin functionally brakes the motor? The block diagram for the DRV8323 does not show everything we need to determine how that signal gets from the INLC pin to brake the motor.

Thanks for the help!