This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV110: Low Side Solenoid/Valve Switcher with current regulation

Part Number: DRV110

Hello,

I am guessing about a component to switch a solenoid with current regulation.

The DRV110 functionalities are ideal for my application, except for peak current. My solenoid has 12V input with 30W power and the only components I can find with theese ratings are full or half bridge drivers.

Unfortunately I can't usa a uC PWM for safety precautions and the component has to drive the coil by itself, as the DRV110 does.

Can you please suggest an alternative to DRV110 with higher current? I can't find anything on the catalog but I am quite confident you can resolve this issue.

I would prefer a derated component, such as 5A peak or higher, if it is possible.

Thanks in advance,


Dario Moscardi