Other Parts Discussed in Thread: DRV8350, INA240, , DRV8353
In the DRV8353x, there are 3 current amplifiers integrated used to sense the low side current. With the all error consideration as offset, gain, temp, how much high resolution it can achieve for motor application?
Input Voltage: 48V
Power Level: 400W
Motor Type: PMSM
If both DRV8350 and INA240 be used in such application, is that resolution better than DRV8353R/H? Very Thanks.
Regards
Brian W