Hi
I have a problem with the DRV8884EVM。when I turn on the power (power of mcu and motor driver),mcu is good running; and then I just set nSleep pin to high, nFault pin changes to low, and keeps low until set nSleep pin to low.
Picture below is gui settings.
VM voltage is 9.6V
VCP is 7.8V
I did not connect a motor.
what problem would lead to vcp is lower than (vm +2)V, how to solve the problem?
Thanks in advance!