This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8884EVM: nFault pin of DRV8884 always be low

Part Number: DRV8884EVM

Hi

I have a problem with the DRV8884EVM。when I turn on the power (power of mcu and  motor driver),mcu is good running; and then I just set nSleep pin to high, nFault pin changes to low, and keeps low until set nSleep pin to low.

Picture below is gui settings.

VM voltage is 9.6V

VCP is 7.8V

I did not  connect a motor.

what problem would lead to vcp is lower than (vm +2)V, how to solve the problem?

Thanks in advance!