Other Parts Discussed in Thread: DRV832X,
Hello,
We are using sensorless motor in our project. we want to use sensorless and 1xPWM Mode. Can we change motor direction with INHC pin?
Thank You
Murat
8.3.1.1.3 1x PWM Mode (PWM_MODE = 10b or MODE Pin = Hi-Z)
The INHC input controls the direction through the 6-step commutation table which is used to change the direction
of the motor when Hall effect sensors are directly controlling the state of the INLA, INHB, and INLB inputs. Tie
the INHC pin low if this feature is not required.