This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2700: DRV2700

Part Number: DRV2700


Hi Sir,

Can we use GPIO with 3.3V to communicate with DRV2700?

The voltage rating below shows there is no maximum value is defined so I assume VIH can be up to 3.3V (up to VDD).

Need your help to confirm it. 

Thanks, Ian.