This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8306: External Comparator

Part Number: DRV8306
Other Parts Discussed in Thread: DRV8304

Hello,

I would like you to confirm about below.

* According to datasheet of DRV8306, this device has "HPA/HNA" for Hall element input.

However, my customer will use external comparator for Hall element due to input voltage range of "HPA/HNA".

(There is possiblity that input range is deviated (1.5V-3.5V) because they will use 12V.)

When I check datasheet, you describe how DVDD can use and connect to HPA/HNA for hall element. But there is no description about external comparator usecase.

So could you please confirm about following my questions ?

Q1. Can user use external comparator ?

      If no, should we change device such as DRV8304 ?

Q2. If yes, could you please show connection example ?

Best Regards,