Hello,
i have a big problem with my DRV2700 piezo driver circuit. Some are working fine and some are not.
Even complete new assembled pcbs have this problem.
Connect the DRV2700 to 5V without enable pin high, everything is as expected. But as soon in set the enable pin high, the DRV2700 gets very fast very hot.
I only have 15V on the output (should be 100V)
I tried lower Vout settings with the same result. I have almost the same layout as the one on the eval board.
Any known issue with the DRV2700 or any other ideas? i am struggling here.
Thank you, best regards
Max