Tool/software: Code Composer Studio
Hello guys,
I'm trying to identify a motor using Instaspin-FOC GUI for the past couple days with no success. I've used several different configurations, such as different pwm and L estimation frequencies and also different voltage and current scales.
It's a turntable direct drive motor that runs at about 20V, star connection and abour 40ohms per phase. The shaft is directly connected to a 3kg heavy metal plate that can't be removed. Normal speed is 90 rpm maximum, and current does not exceed 300ma. The high motor inertia seems to be the problem.
Could someone gime a hint on what parameters to tweek in order to get this motor to succesfully identity?