This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Recommended Stepped Motor Controller and Driver

Other Parts Discussed in Thread: DRV8425, DRV8426

Dear Team,

Could you help to find the suitable stepped motor controller and driver that could meet below requirements for my customer?

Controller

Work voltage

5V

Phase

4-phase unipolar or 2-phase bioplar

Directly

Clockwise/Counter clockwise

Enable

yes

Reset

Initial state

Phase Input

4

Motor drive signal

4

 

Driver

Work voltage

5 ~ 30V

Phase current

under 2A

Drive signal

4

Motor signal

4

Sense

Sense current

Thank you.

Regards,

Jim