Other Parts Discussed in Thread: DRV8323
- The BOOSTXL-DRV8320S EVM is ideally designed as a plug-in module for the MSP430F5529XL LaunchPad development kit. Our aim is to run to a motor with the BOOSTXL-DRV8320S EVM but using a different micro Controller Evaluation module (STM32H7B3I-EVAL). So, is it necessary that we use the BOOSTXL-DRV8320S with only the MSP430 launchpad? Or as long as we provide the required signals from the micro controller evaluation kit to the BOOSTXL-DRV8320S EVM, should we be able to run the motor?
- Also, one of our aims is to also implement FOC. With the BOOSTXL-DRV8320S it is not possible as the current sense is global and not for individual inverter legs. So, are there other EVMs where the low side current sensor is available on all the three inverter legs