Other Parts Discussed in Thread: CSD19532Q5B
Hello,
Similar to this thread (https://e2e.ti.com/support/motor-drivers/f/38/t/877389), the FAULT LED on my EVM board has lit up, and after a power cycle, will immediately light up upon clicking "Start Motor" in the associated DRV8353Rx GUI application. Prior to the fault, I was manually "resisting" the motor from turning during it's default app run. It was set 15A max current, 12V VM, and when it cut power/got overpowered, the motor turned backward ("generated") briefly from the manual resisting torque. Also, the 4 blue LEDs on the ISO-F28028F board "twinkled" slowly after the controller cut driving power.
When powered on, all MOTx terminals = VM (+.5V, which seemed to be the case before the fault as well), all GHx are high, and all GLx are low. Fuse seems to still be in-tact (~0 Ohm when powered off), and VM is still showing 12V in app when powered on.
When powered off, the resistance I am measuring from the MOTx terminals to either VM or GND is ~50kOhm. I see in the EVM schematic that there is ~390kOhm from the MOTx terminals to GND, and the resistance between VM and GND is quite small when powered off (still connected to the power supply though), but I am not sure if 50kOhm is appropriate. I could also measure GHx and GLx when powered off if that is helpful; from what I recall GLx were in the mid-10s of kOhm, and GHx were in the mid-100s of kOhm.
However, after a few power cycles, the FAULT led still turns on, and the Fault Status Register 1 is 0x37F (just GDF fault).
Does the EVM not support "back-driving" during operation? I would think the excess current would get dissipated through the MOSFET body diodes. Is something like an (external) dynamic braking circuit instead required?
Thanks,
Alec