Hello!
I am using DRV8711 in my design for driving high pressure HPLC pumps. We are using several different motors, an one of them, KOLLMORGEN P22NRXC-LNN-NS-D2, enters a resonance at around 1ml/min, which is most used flow, and stepping frequency (1/32 microstep) is around 10kHz. Other motors does not enter the resonance at any rotation speeds.
Is there any guidelines for fighting the resonance?
Current driver settings are:
DTIME = 850ns;
TOFF = 40;
BLANK = 0x0100 + 150;
DECAY = 0x0200 + 20;
DRIVE = 0x00F0;