Dear TI Team
We have received an inquiry from our customers as to whether the DRV8834RGE can be placed in an environment where X-rays are used.
If you look at the website of TI, you will find the following description regarding the regulations under the X-ray environment.
https://www.ti.com/support-quality/reliability/reliability-home.html
”X-RAY information
TI does not typically specify acceptable x-ray levels on the device datasheet. Experience has shown that most TI products will NOT be sensitive to typical x-ray inspection (with typical exposures < 100 rad(Si)). X-ray exposures over these limits, however, may cause damage to the device and should be avoided.”
Is it OK to recognize that when the DRV8834RGE is placed in an X-ray environment, it must comply with the specifications above?
(Or are there any other rules in addition to the above rules?)
Best Regards,
Y.Ottey