This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8912-Q1EVM: Is It posible works in 5V?

Part Number: DRV8912-Q1EVM
Other Parts Discussed in Thread: DRV8912-Q1

hi, i have two arduino, arduno due 3.3V and DRV8912-Q1EVM works good the soleonid, but with arduino atmega2560 (5V)  i cant do work the solenoid, i have osciloscopy and i cant see any thing strange, sclk is in 5V and works and SDI works good in 5V  to bit to bit but the DRV8912-Q1 dont do it noting. i cuted the conexion with the 3.3V and removed all resistences (R9,R10,R11,R11,R12,R13,R14,R15). with arduino due works 3.3V but with ATMEGA2560 doesnt work. any idea? i need that DRV8912-Q1 works in 5V. Thank you.