This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DC motor driver

Other Parts Discussed in Thread: DRV8874

Team,

Do we have H bridge integrated IC could achieve +/-12V voltage. The output current is 5A.

Now customer is using discrete solution.

Roy

  • Hi Roy,

    Thank you for posting to the motor driver forum.

    Do the customer need automotive rated part? My suggestion below is assuming non-automotive. Please let me know if this is not the case.

    • DRV8874 - 37V max, 4.5V min, 6A peak max
      •  Has three control modes (independent half bridge, PWM, Phase/Enable)
      • contains integrated current sensing 
      • 200mohm (High-side + Low-side) RDS(ON)

    You can read more about this part in the datasheet here