This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV110: DRV110 Passive Selection

Part Number: DRV110

Hi everyone,

I would like to use the DRV110 for my solenoid valve application. My calculated parts and application ratings:

Rsens: 0.005 Ohm

Ckeep: 1uF 

Rpeak: 1.2M Ohm

Rosc: 0 Ohm 

Rhold: 285k Ohm

Voltage: 24V

Valve current: 6 Ampers

Please review the values.

Thanks!