Other Parts Discussed in Thread: LAUNCHXL-F28069M, , DRV8323, MOTORWARE, BOOSTXL-DRV8323RS
Hello,
I am trying to spin a BLDC Motor (Trinamic QBL 4208-61-04-013) with the LAUNCHXL-F28069M and the Booster Pack: BOOSTXL-DRV8323RH. I trying to do this for days now with Instaspin and Code Composer Studio 10.
I copied the drivers for the DRV8323 and updated everything accordig to the InstaSpin Quick Start User Guide and the drv8323 firmware.
I compiled the Proj Lab 05b and copied the appProgram.out in the Instaspin-Universal GUI, the motor gets identified, but won't run. Speed_error_RPM is 100%. Bus Voltage is visible.
Is the Combination even possible between the DRV8323RH and the F28069M ? I think DRV8323RH doesn't have the SPI but is Instaspin and the GUI possible to use, nevertheless? Is there some special code I still have to update to use Instaspin without SPI?