Other Parts Discussed in Thread: LAUNCHXL-F280049C, BOOSTXL-DRV8320RS, MOTORWARE, DRV8323, LAUNCHXL-F28069M, , DRV8320
Hi,
we have been developing our system with LAUNCHXL-F280049C and BOOSTXL-DRV8320RS.
In preparation for the next step in development before we have our own PCB we purchased 5 pc BOOSTXL-DRV8323RX
boards with the presumption that it would 'just work' because the chips are identical apart from the on registers which seems to have sensible default values.
Alas, it turns out we made a mistake.
When we tried to run our code we consistently get over current error flag in Instaspin FOC labs.
On investigation we noticed that the nFAULT line is in a different pin on the BOOSTXL-DRV8320RS and BOOSTXL-DRV8323RX.
Is that the only difference?
What do we need to change in the hardware AND software to be able continue with the BOOSTXL-DRV8323RX kits?
We are working based on the instaspin labs for motorControlSKD 3 specifically lab is_07_speed_control.
Having read through and traced the signals in the BOOSTXL interface for number of different LAUNCH and BOOSTXL boards,
not to mention the reading the soucecode and struggling with the always changing pin numbering and conflicting comments and file names
and other inconsistencies in related MotorWare and MotorControlSDKs to say that I'm frustrated would be an understatement...
I noticed in this thread that the boards are compatible but the thread does not say in which way they are incompatible: