Other Parts Discussed in Thread: DRV8353, LM5008
Hi,
As per absolute maximum ratings in datasheet of DRV8353 the max voltage on RT/SD pin should not be more than 7VDC.
I am planning to use single supply so VM and VDRAIN supply will be same that is from a battery rated 60VDC.
In the EVM schematic RT/SD pin is connected to VM via a 274K resistor. In this case voltage on this pin will be more than 7VDC.
Please explain this connection so that I can move further with the design.