This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8847: Pan And Tilt Measurement

Expert 4466 points
Part Number: DRV8847
Other Parts Discussed in Thread: TMAG5170

Hello,

We mounting a sensor to a motor so we can control the pan and tilt after its installed. 

We are planning on using the DRV8847 to drive the motor and using a 3-axis accelerometer to measure pan and tilt. 

Do you have a recommendation for a 3-axis accelerometer and an eval board that communicates via I2C. All we need this for is to calculate the static angle so no special requirements from and acceleration standpoint. 

Are there any integrated motor drivers that will be able to give us this data without an accelerometer? 

Thanks!