Hi team, I have a customer with the following questions:
We are looking into design in DRV8835 motor control IC into our applicaion we had studied the datasheet and have few questions / concerns:
- We are also considering the switch the VCC on and off to enter the sleep mode, so what is the wake time I need to consider?
- Bilk capacitor size and voltage? Please let me know other information you’ll need to help us with the input bilk capacitor capacitance and cap voltage. Our motors are powered by a 2S1P li-poly 300mAh battery pack. The peak current of the motor is around 4A for the duration of 100msec and nominal current is around 1A-2A for 1sec at most.
I can share a schematic snip over email if desired.
Thanks!
-Will