This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2625EVM-CT: In the GUI work mode, what is time of the waveform sequence

Part Number: DRV2625EVM-CT

In waveform sequence, I choose 47Buzz1-100%,what is the time of 47 Buzz1-100%?

What is the time in ms for waveform 47 to run once?

If I want to set up the 47Buzz1-100% run 1s then stop 1s, how to set?

 

BR,

Gust