Other Parts Discussed in Thread: DRV8873, , DRV8873H-Q1EVM
Hello Guys,
Good day.
Just like to inquire if the PWM are set on this device?
Our customer were trying to change the PWM from 0-255, but were unable to do so.
Thanks in advance!
Art
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Guys,
Good day.
Just like to inquire if the PWM are set on this device?
Our customer were trying to change the PWM from 0-255, but were unable to do so.
Thanks in advance!
Art
Hi, Art,
Can you provide the register settings the customer is trying to use?
And, I don't understand what you mean by "Just like to inquire if the PWM are set on this device?" Can you clarify this statement?
Hi Art,
Were you able to get the PWM working? Was the issue with the EVM GUI?
Regards,
Mike
Hi Mike,
I am still waiting for the customers response, but I will let you know guys as soon as I got their confirmation.
Thanks!
Art
Hi Art,
Going to close this for accounting purposes, but feel free to re-open when the customer comes back.
In summary, the DRV8873-Q1 requires an external PWM, and the we generate this signal using the MSP430 MCU on the EVM. The GUI communicates over the USB connection with the MSP430 to set the PWM and duty cycle that is fed to the DRV8873.
Regards,
Mike
It's okay to close the thread Mike.
I'll just create one if ever the customer responded for additional inquiries.
Thanks!
Art
Hello Mike,
Good day.
I just got the response from the customer. He bought drv8873h-q1evm and have specific questions he detailed below in verbatim.
(1) When we apply PWM from 0 to 255 pulses, the board seems to apply the pulses in reverse. 0 generates the highest pulse counts, and 255 generates the lowest pulse counts. Is this the way the board is intended to work?
(2) Which pin is related to DVDD? I am not referring the chip (u3). Rather I am referring to the 14 J1 pins. Which of these are related to DVDD? (I know the pin of u3 is DVDD, but I cannot seem to get access to it).
(3) I am using the Independent Mode. The information below depicts the connections I am using.
1 GND
2 3.3v
3 nFAULT 10Kohm pullup resistor
4 SOD/MODE 200kohm
5 SDI/SR TO GND 53.2v/us
6 sCLOCK/nTRIP TO DVDD (this is connected to external 5v)
7 nSCS/nOL TO DVDD (this is connected to external 5v)
8 EN/N1 PWM/HIGH/LOW
9 PH/N2 PWM/HIGH/LOW
10 DISABLE HIGH/LOW
11 IPRON1 Resistors to convert mirrored current into a voltage
12 nSLEEP HIGH/LOW
13 IPRON2 Resistors to convert mirrored current into a voltage
14 GND
Do you agree this is an acceptable configuration?
(4) One of the methods we are using to control the motor is with a joystick. After initiating movement with the joystick, the board works fine. However, if we release the joystick (return to neutral) too quickly, then we are experiencing a shut down of our power supply. I tried using a diode and am getting the same shut-down effect. Additionally, the board burns at the same time that the power supply shuts down. (We are using a 32v power supply, reduced to 28v). Can you please advise us as to reasons for power supply shut down and boards getting burned?
(5) Inconsistent performance from board to board: I have configured my software to work with the boards. I achieved partial success with one board. However, after burning that board, I install a new one and the new board does not perform like the previous one I was using. For example, the polarity seems to change. With the previous board, I will actuate movement of my motor with a forward joystick push. However, when I connect the second board, a forward joystick push causes the motor to run in reverse. Another example… upon installing the new board and actuating motor movement, the motor reverses direction on its own without a change of direction from the joystick. Can you please advise us on (a) why the boards behave differently, and (b) why we would experience a change of direction in motor movement without a change of direction from our joystick? (Note: we are using an external controller – Atmega 2560)
(6) Is your PWM range from 0 to 255, or 0 to 100?
Thanks in advance!
Art
Hi Art,
Here are some answers and follow-up questions:
1. First to clarify, are we talking about entering the PWM ramp value in the GUI? The 0-255 value is the number of PWM pulses over which the output is ramped to the specified duty cycle. The 0-100 slider is the PWM duty cycle. This should also answer question (6).
2. DVDD is not routed to J1.
3. Configuration seems OK - how is the load(s) connected to the output?
4. Why is the power supply shutting down? Over voltage? Burning out the device could be due to back-EMF when the motor spins down. This will need to be clamped if exceeding 40V (seems like this is the case). This is another question where a simple diagram and description of the loads would be helpful.
5. Again, having an understanding of how the load is connected would be helpful. In independent half-bridge mode, it is assumed one side of load would be tied to GND or VM supply, so should not be seeing a change in direction since we can only move in a single direction. Read page 16 of the datasheet. Not sure if there is a single motor connected across OUT1 and OUT2 - this is not desired in independent half-bridge mode, and could explain why devices are getting burned up.
6. Please see (1).
Regards,
Mike
Hello Mike,
Apologies for the delayed response for I was awaiting the info from the customer. He do have follow-up inquiries. See below.
1) You mentioned DVDD is not routed to J1. SO can he use an external 5v signal instead of DVDD?
2) On page19 of the datasheet for DRV8873-Q1, The IPOPI1 and IPROPI2 they are connected together, Will this configuration works for all the MODE's ?. Also, Does he need to add an external Rsense-1 ?
Thanks to confirm!
Art
Art,
1) DVDD is an internally regulated voltage on the DRV8873-Q1, so we don't bring it out to a connector. It is not intended to drive more than 2mA of current per the datasheet. It should NOT be provided externally.
2) Please read the text above figure 14 of the datasheet and it should be clear. These are connected together to sum the currents of each half-bridge. If that is not desired, the pins should be separated and a resistor should be placed on each IPROPI pin (this is shown in figure 12). If they are connected together, only a single resistor is needed.
Please read section 7.3.1.3 completely to understand how the external resistor is calculated based on current in the load.