Dear support team,
I have the confirmation about the external capacitor on SO pin of DRV8703-Q1.
On the specification sheet, it describes "No capacitor is required on the SO pin." on "7.3.5 Amplifier Output (SO)".
On the other hands, it describes "Place an external capacitor on this pin." on "7.3.5.1 SO Sample and Hold Operataion".
Does this mean that if we set SH_EN : Low (default), no capacitor is required on SO pin, and if we set SH_EN : High, need the capacitor on SO pin?
And, in that case, if we set SH_EN : High, is your recommended value 1nF?
Best Regards,
Matsunaga