Hi Team,
One quick question.
Regarding the Cap for the CP, datasheet says as below. I understand TI recommends 0.22uF rated value but effective value is varied depending DC biasing, right? So my question is "how much effective value(at what voltage) is need for safety operation of DRV8818?"
Recently, ceramic cap is getting smaller due to suppliers strategy and effective value is also getting smaller at same voltage level due to the size down.
A low-ESR ceramic capacitor must be placed in between the CP1 and CP2 pins. TI recommends a value of 0.22-μF rated for VM. Place this component as close to the pins as possible. A low-ESR ceramic capacitor must be placed in between the VM and VCP pins. TI recommends a value of 0.22-μF rated for 16 V. Place this component as close to the pins as possible.
Regards,
Takashi Onawa