Can you confirm that the spi_step can be used to do everything the the external step pin can do, also with the dir pin I can just use the spi_dir bit setting instead?
Reason is to save IO lines in the design , if I can do it through the spi bus it will be easier from a pcb point of view.