Hi Sir,
My customer using DRV8876 test case temperature around 50 degree C in ambient temperature condition.
Do you think it looks a little bit higher?
Thanks, Ian.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,
My customer using DRV8876 test case temperature around 50 degree C in ambient temperature condition.
Do you think it looks a little bit higher?
Thanks, Ian.
Hi Ian,
It is possible to reach those temperatures If the board layout has not been optimized for good thermal dissipation. Poor thermal dissipation may cause the temperature to greatly increase.
Is the customer using their own board design or the DRV8876EVM?
Is the output current measurements RMS or peak values (constant values)?
Hi Sir,
It’s in customer’s PCB measure RMS current.
May I know how to calculate thermal according measure current value?
Thanks, Ian.
Hi Ian,
This application note explains how to calculate power dissipation. When calculating power dissipation, you have to consider the RDS(on) power dissipation and switching loss. In this case, the RDS(on) dissipation can be calculated as follows: 2*0.350*0.598^2=0.250W. The switching loss, assuming 20kHz frequency, is roughly equal to 0.0126W which is very small compared to the RDS(on) power dissipation. So the largest contributor of power will be the from RDS(on) unless the customer is switching at a much higher frequency.