Other Parts Discussed in Thread: DRV8323
Tool/software: Code Composer Studio
Hi everyone,
I would like to motorize a longboard with this motor driver "BOOSTXL-DRV8323RS". But I don't find suitable motor to this controller. The closest motor I found has this characteristics : Max current 80A, Max voltage 41.5V, 1550W. My controller has the following characteristics : 6-54V and 15A. I am wondering if the motor driver BOOSTXL-DRV8323RS is enaught for this motors. I mean will the driver restrain the capacity of the motor ? .Or do I have to change the motor for another one ? If yes do you have references ?
Sincerely,
PERRIN Paul-Emile