This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2604L: DRV2604 auto calibration failed / overcurrent

Part Number: DRV2604L


Hello,

we are using a DRV2604L with the LRA C08-00A.003 (Precision Microdrives).

Supply Voltage of the system is at approx. 2.8V

LRA Parameters: Rated voltage: 1.2V, Frequency: 240Hz

Unfortunately, we are not able to run an autocalibration, we habe done the sequence described in the datasheet at p. 27 und get the status register result OC_DETECT=1 and DIAG_RESULT=Auto-calibration failed. LRA does not vibrate.

Schematic:

We have probed the voltage at OUT+ after setting the GO for autocalibration, showing the following results:

Written register contents are:

Addr 0x01 = 0x07

Addr 0x1A = 0x96

Addr 0x16 = 0x2E

Addr 0x17 = 0x3A

Addr 0x1B = 0x90

Thanks for your reply.